{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is BS number, short circuit capacity and maximum Zs values on an installation which has SFH3040 circuit breakers?
The BS Number is BSEN60947-2 and breaking capacity is 65kA.
Attached file includes maximum ZS values, but In order to comply with BS7671 Amendment 3: 2015, the figure in the attachment should be multiplied by Cmin of .95

Schneider Electric Ireland

Attachment(s)
Trip curve Zs SF,K,L,M,N,P.pdf [26.1 KB]