{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Was the pressure switch ACW6 made obsolete? What can I use as an alternative?
Yes, the ACW6 pressure switch of the 9012 range is no longer available.

The alternative will depend on the desired set point.

The ACW6 had a range setting of 5.4..34 bar so it can be replaced by either:

- ACW2 if set point below 20 bar
- ACW7 if set point above 20 bar

Below are the full specs of the three units:

ACW Catalogue

Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.