Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to install/remove NSX mccb from powerpact 4 panel and the torque settings required.


When installing a PowerPact 4 MCCB onto the panel, the shear off bolts will shear when the correct torque setting has been reached - 20Nm for 100/160/250 frames and 28Nm for 400/630.

Refer to the instructions below, which are from the attached file.

Instructions

PP4 installation

A 17mm bi hex socket tool is required for removing the MCCB after the shear off bolts have been removed during first installation.

Schneider Electric Ireland

Attachment(s)
PP4 Panel Instructions 75210222A Rev B.pdf [6.64 MB]