המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does Schneider offer a 8910DPA contactor with 4 normally closed power poles?
Issue:
Contactor with 4 normally closed power poles

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8910 Types DP/DPA Contactors

Cause:
Normally closed contacts required

Resolution:
No we do not offer a definite purpose contactor with 4 normally closed poles.
We have a 4-pole contactor that has 2 normally open and 2 normally closed.