המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the duty cycle for the ATS48 unit?
Issue:
ATS48 duty cycle

Product Line:
ATS48 soft starts

Environment:
Duty cycle

Cause:
n/a

Resolution:
In standard duty applications, the ATS48 soft starter is designed to provide: Starting at 400% of IN for 12 seconds, or 300% of IN for 23 seconds, with a load factor of 50% and 10 starts per hour or an equivalent thermal cycling.
In severe duty applications, the ATS48 soft starter is designed to provide: Starting at 400% of IN for 48 seconds, or 300% of IN for 90 seconds, from a cold state Starting at 400% of IN for 25 seconds with a load factor of 50% and 5 starts per hour or an equivalent thermal cycling the motor thermal protection conforms to Class 20 thermal overload protection.