המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can the drawing for the enclosed ATS48 be obtained?
Issue:
Could not find the drawings for Enclosed Softstarts.

Product Line:
Enclosed Softstart 48

Environment:
All Enclosed Softstart Models

Cause:
N/A

Resolution:

The drawings for the enclosed products can be downloaded from the technical library section of the Square D website.
Otherwise, contact your Square D distributor or filed office with the factory order number from the nameplate of the product. They should be able to obtain specific drawings from the Square D plant that built the unit.