המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is included with the Class 9998 Type S contact kits?
Issue:
9998 contact kit parts

Product Line:
Type S Accessories and Components

Environment:
Contactor and Starter Replacement Part Kits

Resolution:
The 3 pole contact kit will contain - 3 moveable contacts, 6 stationery contacts and 6 stationery screws.
***Springs are not included because part of the contact carrier assembly.

NOTE - 1 pole contact kit is 1 set of NO power pole contacts
- 2 pole contact kit is 2 moveable contacts and 4 stationary contacts with screws
- 4 pole contact kit is 3 moveable contacts and 6 stationary contacts with screws plus a set of NO power pole contacts.  The 4th pole power contacts are different from the normal starter contacts.