המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the replacement drive part number for a Variable Torque Drive?

Issue:
Looking for the replacement drive part number for a Variable Torque Drive.

Product Line:
ATV Altivar Process

Environment:
All

Cause:
Selection

Resolution:
Altivar Drives are no longer referred to as constant or variable torque, however, these drives are intended for fans and pumps more than other applications.   Altivar 212, Altivar 320, Altivar 600, Process Altivar 660 are the current suggested drives for fans and pumps.