איך נוכל לעזור לך היום?

Is there a password protection available for restricting access to the ATV61 or ATV71 display parameters?

Issue:
Password protection set-up for ATV61 or ATV71

Product Line:
ATV61 ATV71

Environment:
All

Cause:
Parameter access

Resolution:
No. The Password protection available is for Upload and Download rights. However, user can limit parameter access by setting Access Level to desired setting and by selecting or deselecting parameters in the Display Config menu using Parameter Access.