איך נוכל לעזור לך היום?

What are the Differences between Motor Circuit Breakers of types GV2ME and GV2RT ?

Both GV2ME and GV2RT are Thermal Magnetic Motor Circuit breakers (that don't need external Thermal overload relay),

The Main Differences are found in the following points:

- GV2ME:
- Control is done by Push buttons
- It is used with Motors with motors of normal applications

- GV2RT:
- Control of the CB is by Rocker Lever
- It is used Mainly with special motors of high Peak Current on starting rather than normal applications