איך נוכל לעזור לך היום?

What's the difference between IP & IK standards?

IP standards are user to describe the degree of protection of objects against solid bodies and liquids. The first number describes the protection against solid bodies, while the second number is for the protection against liquids.
As for IK standards, they're used to describe the protection of objects against mechanical impacts.