המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What are the trip curves for the ATS48?

Issue:
Looking for the trip curves for the ATS48.

Product Line:
ATS48 soft starts

Resolution:
The ATS48 controller is preset to provide Class 10 thermal overload protection for standard duty applications. The ATS48 controller can be adjusted to provide Class 2, 10A, 10, 15, 20, 25, or 30 thermal overload protection, as necessary. Each class of overload follows a different trip curve. Additionally, there are different curves used for cold start and for hot start. These charts are listed on pages 40 and 41 in the instruction bulletin, S1A37491 dated 01/2010.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.