המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PowerChute Business Edition events are not being logged to the Windows Application Log.
Issue:
PowerChute Business Edition events are not being logged to the Windows Application Log.

Product Line:
PowerChute Business Edition, prior to v9.1.1

Environment:
All supported Windows OS with Java versions
7 update 21 or later
6 update 45
5 update 45

Cause:
Changes by Oracle to latest Java versions

Solution:

Upgrade PowerChute to the latest version available at this link http://www.apc.com/us/en/tools/download/​

NOTE: If you are running a version of PowerChute Agent prior to 9.1.1, and you use the JRE Configuration Tool to upgrade to a JRE version HIGHER than any of the following, PowerChute stops writing events to the Windows application log:
  • Java 7 update 21
  • Java 6 update 45
  • Java 5 update 45