המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the part number for the ATV71HC11N4 and ATV61HC13N4 power boards?
Issue:
Needs a Power board for ATV71HC11N4

Product line:
ATV71 and ATV61

Environment:
All models, all serial numbers

Cause:
Power board not functional

Resolution:
The Power board for these drive is VX5A1HC1113.

It is required to check the Serial number of the drive before ordering the Power Board.
If the 8th digit in the serial number is 2, the drive was built using Fuji IGBT's instead of the standard Mitsubishi IGBT's.   A drive with Fuji IGBT's requires a modified version of the Power board (VX5A1HC1113F).   IGBT, and gate driver board parts also will have an F at the end.