המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Which S-flex 212 drives have fusible disconnect or circuit breaker?

Issue:
Customer needs to know which S-flex 212 drives have a fusible disconnect or circuit breaker?

Product Line:
ATV212 S-Flex

Environment:
ATV212 (1 hp-100 hp S-Flex)

Cause:
Which enclosed units have fuses and which come with circuit breakers?

Resolution:
All of the S-Flex drives will have circuit breakers for short circuit protection except the 460VAC 75HP, 100HP SFD212RG4 and SFD212SG4.  These two will have a fusible disconnect.

Note: All of the 460VAC units will have power fuses and circuit breakers except the 75HP and 100HP that will not have the circuit breaker but only fuses.