המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the minimum cancelling time of the power supply voltage for the Sepam 2000 without its reinit (restart)?

Effects of interruptions of the DC power supply. (IEC 60255-11)
The effects are determined for an interruption with a duration chosen in the following list and declared by the manufacturer : 2 _ 5 _10 _ 20 _ 50 _ 100 _ 200 ms

The interruption must be sudden, i.e.the auxiliary power supply must vary from 0 to the rated value and the opposite .

The relay must not change erroneously its output status when the power supply value is applied or cancelled.

Fugitive cancellings Sepam 2000:
75 ms to Vsupply = Vnominal
30 ms to Vsupply = Vmini

Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 2000

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166857 V2.0, Originally authored by FrKr on 06/18/2008, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 20