המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
From the display, how do I set the voltage transformer settings (VT settings) in a Series 20 Busbar Sepam 1000+?

From the main front screen, press the button that looks like the face of the Sepam 1000+ until the VT settings (General Charcteristics) screen appears. You will be prompted for a password. The default password is all 4 zeros.
1

Original article#3634
Last Revised: 17 June 2008 by DRM

Applies To: Sepam 20, Sepam 1000+

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL184564 V2.0, Originally authored by DaMi on 06/16/2007, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 20