המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Could you clarify the meaning of "PUP" in the Comtrade file of SFT2826?

PUP is the "pick-up" of the fault. Often people mistake "PUP" as the pickup of disturbance recording, but this is incorrect because the disturbance recording is often configured with pre-trig cycles that are used to view the recording before the actual disturbance. "PUP" relates to the instantaneous pickup of a protection function, input, control logic or any other condition that sends a tripping order to the CB. This information is very useful when analyzing a comtrade file because it helps find the origin of a sepam trip and system shutdown.

Re-published to revised security level: 20 June 2008 by DRM

Applies to: SFT2826

Internal PMO/PMC Support

All content © 1992-2007 Schneider Electric

AEDL3




Legacy KB System (APS) Data: RESL188980 V2.0, Originally authored by KBAdPM on 11/08/2007, Last Edited by DaMi on 06/21/2008
Related ranges: SFT 2826 (OPG display)