המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Which protocols can be used on SLAN output (Fiber optic output) of ACE969FO-2?

ACE969FO-2 SLAN output is a serial port only and therefore only supports serial protocols. In this case, these protocols are Modbus RTU, DNP3 and IEC60870-5-103 protocols. Since Modbus TCP/IP is an Ethernet protocol, it is obviously not supported by the ACE969FO-2 serial communications accessory.
For more information, there is a chart in the "Communication Accessories" section of the Sepam 20, 40, 80 "Digital Protection Relays" catalogue. A copy of this chart from the 2010 version of this catalogues is reproduced below for convenience:

reference1


Keywords: Ethernet communications, serial communications, fiber ethernet, fiber serial, fiber optic, connection port, support, Modbus RTU over Ethernet, DNP over Ethernet, IEC103, Modbus TCP

AEDL3




Legacy KB System (APS) Data: RESL199704 V3.0, Originally authored by DaMi on 08/26/2009, Last Edited by DaMi on 02/02/2010
Related ranges: ACE 9XX