המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATV31 : Remote terminal VW3A31101, LCC in CtL menu, how to do a run reverse command/order with keypad?

Issue:
ATV31 : Remote terminal VW3A31101, LCC in CtL menu, how to do a run reverse command/order with keypad?

Product Line:
Altivar ATV31

Environment:
All serial numbers, all model numbers.

Cause:
Customer can't do a run reverse with deported keypad, but can do the run forward

Resolution:

By default, the only authorized direction is forward.
To be able to run also in reverse direction, the parameter ROT (in Ctl menu ) must be Set to the value "Bot" (for both directions)

Note : The parameter ROT appears in Ctl menu ONLY if the control is taken by LCC.