איך נוכל לעזור לך היום?

Why don't I see my sections after converting a project from Concept to Unity Pro?


The most likely reason is that the Concept project was exported from the Concept converter with the Option " Project with used DFB's ( Re-Connect to Equal ) "
This is not supported in Unity Pro and your sections will not convert.
Re-export the project from the source PC with the option " Project with used DFB's "



Legacy KB System (APS) Data: RESL171628 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro