המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to move the ProWORX 32 authorization using a USB memory device.

Goals and Symptoms

To move the ProWORX 32 authorization from a Source PC to a Target PC using a USB memory device.

Causes and Fixes

To move the ProWORX 32 authorization from your PC to a USB memory device, follow this procedure.
Launch the ProWORX 32 Authorization wizard from your PC and click on the "NEXT" button to continue.

img1

Choose the option for "Transfer Authorization" and click on the "NEXT" button.

img2

Choose the option for "Transfer authorization from computer to disk". Select the drop down menu and choose the drive that supports your USB memory device. Click on the "NEXT" button to continue.

img3

The authorization should now be transferred to your USB memory device. Click on the "Finish" button.

img4

To move the ProWORX 32 authorization from your USB memory device back to a PC, follow this procedure.
Launch the ProWORX 32 Authorization wizard from your PC and click on the "NEXT" button to continue.

img5

Choose the option for "Transfer Authorization" and click on the "NEXT" button.

img6

Choose the option for "Transfer authorization from disk to computer". Select the drop down menu and choose the drive that supports your USB memory device. Click on the "NEXT" button to continue.

img7

The authorization should now be transferred back to your PC. Click on the "Finish" button.
img8