Installing the new MBX Driver for the TSXCUSBMBP Communication Adapter.
Goals and Symptoms
Installation of the new Driver (MBX Driver version V6.00 Update 20070615) for the TSXCUSBMBP adapter.
Causes and Fixes
If the TSXCUSCMBP VSP driver was installed it will need to be uninstalled.
After uninstallation of VSP driver then install the MBX driver.
See attached for both procedures.