איך נוכל לעזור לך היום?

TSX CAYxx – Uncertain reconfiguration of channels at the power ON

At the power-on, the User has to Check the state of the bit "RECONF_IN_PROGR" (%MWr.m.c.0.15).  If this bit is at 0 before, start Read_Param.