המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the minimum version of the Unitelway driver required to use the USB cable (TSXPCX3030 or TSXCUSB485)?

Issue:
Minimum version of the Unitelway driver required to use the USB cable (TSXPCX3030 or TSXCUSB485)

Product Line:
TSXCUSB485, Unitelway

Resolution:
To use the USB cable (TSXCUSB485 or TSXPCX3030) your Unitelway must be Version 1.8 or later.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)