המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to unlock "Generic Windows PC Series" as a Target Type in Vijeo Designer?

Article available in these languages: Spanish

Issue:
Unlocking the Generic Windows PC Series target.


Product Line:
Vijeo Designer


Resolution:
To unlock the Generic Windows PC target type. You need to go to the Help Menu and select "About..."

Under the License tab select the "Upgrade.." button. Input "VJDHTGTSPVxxM" in the Upgrade Reference
Number field. (where xx denotes the version of Vijeo Designer, if you are running V6.0 use "60" in it's place.)


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)