איך נוכל לעזור לך היום?

Cannot find the MIB files for the BMXNOC0401.

Issue
Cannot find the MIB files for the BMXNOC0401.

Product Line
BMXNOC0401

Environment
Windows 10

Resolution
There are no MIB file on the NOC because it does not use a private mib. The NOC uses standard MIB's.

Private MIB's require the use of a file to define data types and structures.