המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can I setup Vijeo Citect to communicate to a controller via Modbus Plus using the TSXCUSBMBP adapter?

This documents explains the steps involved in configuring Vijeo Citect to communicate to a controller via Modbus Plus protocol.

This procedure uses the Vijeo Citect MBPLUS Driver.

1) Configure the I/O Server, Boards, Ports and I/O Devices as shown below:image

2) Testing with a Quantum / Unity Controller which requires to select the MBPLUS20 Protocol.image2

Attachments

3) Install the latest version of the MBPLUS driver.  Note: you will need to install the latest version of the Modbus Plus MBx driver.