המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is it possible to zoom in on a Vijeo Designer WebGate session?

Issue
Is it possible to zoom in on a Vijeo Designer WebGate session to make box where the HMI panels are shown larger?

Product Line
Vijeo Designer all versions - Web Gate

Environment
Microsoft Edge with Internet Explorer mode active viewing WebGate

Resolution
The pixel resolution of the WebGate screen will be fixed to match that of the physical HMI screen no matter how much you zoom in the browser window itself.

However, here are a few suggestions to help:

[1 - Change Windows Display resolution]
Lower the screen resolution on the monitor through Windows Display settings

[2 - Windows Magnifier]
Launch the built-in Magnifier Tool in Windows.

In Windows 10/11, here's a guide on the controls and settings
https://support.microsoft.com/en-ca/help/11542/windows-use-magnifier

[3 - Use a Third-party Magnifier software]
Here is an open source magnifier tool for example - Virtual Magnifying Glass 3.7
http://magnifier.sourceforge.net/