המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to use the Serial recovery cable for XBTGT terminals

Goals and Symptoms

How to use the Serial recovery cable for XBTGT terminals

Causes and Fixes

To use VJD Runtime installer in recovery mode for XBTGT, it is necessary to use the serial recovery cable and to follow these steps:

-Put the Dip Switch 3 to ON position in your XBTGT
- connect the XBTGT to your PC by the serial recovery cable and Ethernet or USB cable at the same time.
- start the Runtime installer, select your XBTGT series, select the recovery mode and click in send button
- turn the target machine on.


Legacy KB System (APS) Data: RESL180553 V2.0, Originally authored by on , Last Edited by JaOu on 11/28/2006
Related ranges: Magelis XBT GT