איך נוכל לעזור לך היום?

The Lexium ILx runs OK in open loop; in closed the motor keeps stalling.

Possible problem and solution:

Be sure the move profile adjusted to encoder counts when EE=1.
The stall factor (SF) may be to low.
Increase to SF=20.
This will help eliminate nuisance trips.
Depending on the application stall factor, adjustment may be needed based on acceptable position tolerances.


Legacy KB System (APS) Data: RESL200079 V1.0, Originally authored by MaPr on 09/25/2009, Last Edited by MaPr on 09/25/2009
Related ranges: Lexium ILT, ILP