המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
The manual states the drive has built in ground fault detection that can be disabled in expert mode. What is the ground current limit to trigger this condition and the fault error number that will result when the ground fault is detected.

Goals and Symptoms

The manual states the drive has built in ground fault detection that can be disabled in expert mode. What is the ground current limit to trigger this condition and the fault error number that will result when the ground fault is detected.

Causes and Fixes

The errormessage is E2300 (overcurrent amplifier).The current limit is < 10A.


Legacy KB System (APS) Data: RESL202246 V1.0, Originally authored by KlWo on 05/11/2010, Last Edited by KlWo on 05/11/2010
Related ranges: Lexium 32