המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Lexium05B / SD328B - Profibus What means errorID B30F hex ?

Goals and Symptoms

Lexium05B / SD328B - Profibus

What means ERROR ID "B30F" hex ?

Causes and Fixes

B30F hex means "Profibus: faulty processing of process data channel"
This problem occurs if the profibus master PLC send an ENABLE command when the drive is in state 3.
State 3 means DISABLED ( STO inputs are FALSE or main supply is missing)
Before calling MC_Power.Enable = TRUE the drive state should be checked if it is in state 4 (ready to switch on).


Legacy KB System (APS) Data: RESL202776 V1.0, Originally authored by StKu on 06/30/2010, Last Edited by StKu on 06/30/2010
Related ranges: Lexium 05