איך נוכל לעזור לך היום?

Commissioning problems with Berger Lahr N065 / IclA N065 IXXAT USB-CAN compact interface running with the BLCT IclA software.

Goals and Symptoms

Commissioning problems with Berger Lahr N065 / IclA N065

"IXXAT" USB-CAN compact interface running with the BLCT IclA software.

Causes and Fixes

ICLA-CCT / BLCT --> "IXXAT USB-CAN".

To communicate with a IclA D065 drive use the "Ixxat" driver version 2.16x !!!
The BLCT for N065 supports only the "IXXAT VCI V2" driver.

( VCI Driver from "IXXAT" has to be installed )

שניידר אלקטריק ישראל

קבצים מצורפים
Changing_Driver_version_for_IXXAT_USB_TO_CAN_from_VCI_V3_back_to_VCI_V2.zip [338.11 KB]