המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the pinout of the TSXPCU1030, TSXPCU1031 programing cable?

image0

8 Pin mini-din
1. D (B) RS 485
2. D (A) RS 485
3. Not Used
4. Negative Data Transmit Enable
5. TER port mode control
6. Not Used
7. GND 0V
8. Logical VCC

9 Pin SubD
1.DCD
2. Rx
3. Tx
4. DTR
5. Signal Ground
6. Not Used
7. RTS
8. CTS
9. Not Used

User-built cables are possible, but not recommended. An example below of a user-built cable employing a B&B Electronics RS232 - 485 converter (MN: 485LDRC) is shown below:
image1

The dip switches on the converter are set to as follows:
1 Up, 2 Up, 3 Up, 4 Up, 5 Down, 6 Up, 7 Down, 8 Down

Legacy KB System (APS) Data: RESL162737 V1.0, Originally authored by on , Last Edited by on
Related ranges: Uni-Telway