המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can a Unity Quantum project be converted to a Unity Premium project?

Issue

Can a Unity Quantum project be converted to a Unity Premium project?

Product Line

Unity Pro, Quantum, Premium

Environment

Unity Pro v8.0

Resolution

No, the two product lines support different IO and different instruction sets. This type of conversion is not available. Converting a Unity Premium project to a Unity Quantum project is also not possible for this reason.
The Schneider Electric recommendation is to upgrade for a M580 controller using the Unity to M580 Converstion (UMAC) tool.