המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to Install the M1-Advantys.mdc File to Concept

Issue
This Resolution describes the steps required to install the M1-Advantys.mdc file into Concept.

The attached MDC (M1-Advantys.mdc) file is used exclusively with Concept Programming software to allow Momentum processors to operate Advantys Islands on a Momentum IO Bus network. An Interbus NIM (STBNIB2212) is the interface used on an island communicating on the IO Bus network.


Product Line
Momentum


Environment
Concept


Resolution

When mapping Advantys Islands on an IO Bus network, do not use the Generic map '170-IOBUS-xxx'. Instead, always use the compatible 'Advantys-0xxx' selection. If a Generic IO map is selected for an Advantys island, all inputs will read as zero if an input or output fault occurs on that module. With the 'Advantys-0xxx' selected, inputs will be read normally if an input or output fault condition occurs.

When changing the configuration of an island by adding or removing modules, the drop must be reconfigured using the Advantys Configuration Software. When using the Auto-configuration button on the front panel of the NIM, power down the island and make the changes by adding or removing the modules. Power-up the island and push the auto-configuration button. When auto-configuration is complete, power cycle the island.

שניידר אלקטריק ישראל

קבצים מצורפים
M1-Advantys.zip [903 Bytes]