המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
STBNIP2212 Advantys Ethernet NIM Firmware Upgrade to version 2.2.7, Web Upgrade to version 1.19.6

Issue
The purpose of this resolution is to inform STBNIP2212 users that the firmware has been upgraded to version 2.2.7. To utilize the additional functionality, the web pages have also been upgraded to version 1.19.6 and should be installed after firmware  v2.2.7 is installed. The primary feature of this upgrade is the addition of Faulty Device Replacement (FDR) services which are explained in the attached documents.

Firmware version 2.2.7 is field upgradable and will operate with any STBNIP2212 Kernel version.


Product Line
Advantys
STBNIP2212


Resolution
The following upgrades and changes were made to Exec v. 2.2.7 which are discussed in further detail in the attached FDR document.
1. A revised IP address assignment process for Bootp and DHCP
2. Multiple FDR servers
3. FDR Functionality
4. Device Parameter file backup/restore
5. FDR Diagnostics
6. Discrete Output behavior configuration