המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
USB style connectors of M340 and Unity Quantum programming cables

Goals and Symptoms

Quantum 140CPU6xxx0 CPUs and M340 CPUs USB style programming cable connector description.

Facts and Changes

5-pin Mini B USB Type for use with M340 Processors
Mini b


4-pin Mini B USB Type for use with Quantum 140CPU6xxx0 Processorsmini b

Causes and Fixes

The M340 USB programming cables are BMXXCAUSBH018 (1.8m) and BMXXCAUSBH045 (4.5m) which have a USB Type mini B 5-pin connector. The Quantum USB programming cable is UNYXCAUSB033 (3.3m) which has a USB Type mini B 4-pin connector.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)