המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to achieve software calibration with TSX ISPY101 ≥ SV2.2? (July 2011)

Goals and Symptoms

Enhancement for TSXISPY101 SV2.2 or greater.
These enhancements are referring to software and forced calibrations, to use Unity Pro V6.0 or greater is required.

The goal of this resolution is to give you all information for dealing better the calibration by program.

Causes and Fixes

Attached below is a tool to perform calibration (.ZEF file to use in Unity Pro directly).

In this file is the complete process about the normal, software and forced calibrations: use the operator screens (information included inside). Launch the calibration menu and navigate under dedicated operator screens.

There's also a functional module (.XFM) that you can import in the application when the project functional view is displayed.

שניידר אלקטריק ישראל

קבצים מצורפים
Application_for_software_calibration_with_TSXIPSY101_SV2.2_or_higher_b.zip [382.52 KB]