איך נוכל לעזור לך היום?

Error 108 when upgrading ION7300 meter firmware

Issue

Firmware upgrade fails with error 108 repeatedly.

Product Line

ION 73xx

Cause

When upgrading an old firmware of ION7300 meter i.e. v113 to latest Rev A v213, the upgrade keeps failing with error 108.

Resolution

Increase the "Receive Timeout" of the device in the Management Console from 1800 to 7200 and this should work.