המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
MV-90: Meter Events


Question

How do I retrieve meter events and decode the events MV-90 reports?


Answer


The TIM automatically reads the meter Event Log for the same time period an All/Partial read is performed.

To retrieve events:

-Perform an All/Partial Read

-Meter Events -> Event Maintenance -> Choose RecorderID

-Change the Start Date to an earlier date -> Go

Event Codes and descriptions do not match the events recorded in the meter, and not all events are retrieved from the meter.

Look at the latest TIM_Appnote in C:\MV90xi\TIMs for conversion of ION events to MV-90 events.

Original Article#16576
Last Revised: 23 March 2008

Applies To: MV90 Software

Original Author: Ali Beittoei

Internal PMO/PMC

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL192303 V1.0, Originally authored by DaMi on 07/13/2008, Last Edited by DaMi on 07/13/2008
Related ranges: MV90