המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Power Monitoring Expert : Database Maintenance Task Schedules

Issue

What are the default schedules for the scheduled jobs in Power Monitoring Expert?

Environment
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.x, 8.x, 9.0, 2020

Resolution

The following Windows Scheduled Tasks are present in SPM systems as of version 7.0.1. The following table shows all the available scheduled task by type of installation and their default execution times.

Task NameSystemSchedule
[ION_Data] - BACKUP - JobSQL ExpressEvery Friday at midnight.
[ION_Network] - BACKUP - JobSQL ExpressDaily at 1:00 AM
[ION_Data] - MAINTENANCE - JobSQL ExpressDaily at 2:00 AM
[ION_Data] - SIZE NOTIFICATION - JobSQL ExpressDaily at 3:00 AM
[ION_Network] - MAINTENANCE - JobSQL ExpressDaily at 7:30 AM
[ION_SystemLog] - TRIM - JobSQL ExpressDaily at 4:00 AM
[ION_SystemLog] - MAINTENANCE - JobSQL ExpressDaily at 7:05 AM
[ApplicationModules] - MAINTENANCE - JobSQL Express and StandardDaily at 3:30 AM
[ApplicationModules] - TRIM - JobSQL Express and StandardDaily at 2:30 AM
[ApplicationModules] - BACKUP - JobSQL Express and StandardDaily at 1:30 AM

FAQ - FA233177 explains "How to modify database maintenance schedules contained in Windows Task Scheduler".