המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does the Device List need to be configured in the EGX / ECC setup page?

Product Line
EGX300
EGX400
EGX200
EGX100
EGX150(Link150)
ECC21

Environment
Device List

Resolution
The EGX series and ECC series of gateways do not require the user to modify the device list as long as all devices are Modbus and not a mix with Powerlogic and jbus. Port 2 of the EGX200 and EGX400 however must have a device list set.

The EGX300 has a Device Auto Discovery mode which will go out and determine which devices are on the chain for the user and auto-populate the device list.