How to Connect RS-485 wires that have different port labels
Issue
Some RS-485 ports are labels can differ between meters
Product Line
PowerLogic & ION circuit metering
Environment
Power Monitoring
PowerLogic & ION installation
Cause
The two conventions shown below:
- A, B, SH
- (-), (+), SH
Resolution
The two label conventions link to each other as below:- A = (-)
- B = (+)