המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ION Setup Installation Error: "Can't run 16-bit Windows Program"

Goals and Symptoms

ION:Setup pops up a error during the initial installation screen (see below) indicating that a file cannot be written to a temp directory.

Facts and Changes

After double clicking on Setup.exe (to install ION:Setup) the MSI install wizard appears. Once the user clicks the Next button a error popup appears as below:

Error reads:

  • Can't run 16-bit Windows program
    Cannot find file ...\Local Settings\Temp\pft80.tmp\Setup.exe (or one of it's components). Check to ensure the path and filename are correct and that all required libraries are available.

Causes and Fixes

Check that the login provided has local administrator rights (user has been added to the local administrators group). Next check the folder permissions are set for Full Control permissions in the following location:

C:\Documents and Settings\<User Account>\Local Settings\Temp

NOTE: This folder is a hidden directory, so you may need to change the folder options to 'show hidden files and folders'
(in Windows Explorer) Tools -> Folder Options -> View (tab)

This should allow you to complete the installation process successfully.




Last Revised: November 16, 2007
Applies To: ION Setup
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189282 V1.0, Originally authored by KBAdPM on 11/17/2007, Last Edited by KBAdPM on 11/17/2007
Related ranges: ION Setup 2.1, ION Setup 2.0