המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is it possible to get data from a 3rd-Party Microsoft SQL Database into ION Enterprise's VIP?

It is sometimes desirerable to get data from a database that is not part of ION Data into ION Enterprise, so that the Arithmetic Module in the VIP can be used for calculations and reporting.


  • This is possible. Lets say, for example, the user wants to get data from a 3rd party database into VIP and then do some kind of arithmetic calculation on it.

    The easiest way to do this is:
    • Move the data from SQL to Excel
    • Use an Excel OPC Server and the ION OPC Client to bring it into the VIP

    NOTE: The ION OPC Client is considered 'custom', and requires an Application Engineer to configure. Please contact your Sales Representative for more information.


Last Revised: December 7, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL190281 V1.0, Originally authored by KBAdPM on 12/07/2007, Last Edited by KBAdPM on 12/07/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0