המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Viewing the VAUX on the 3720 ACM Front Panel Display

The VAUX input of the 3720 is not viewable, by default, on the meter's front panel display. To view this parameter, you will need to configure the meter as follows:

  1. Connect to the 3720 in ION:Setup (Network setup mode).
  2. Double click on the Group Keys option.
  3. It is your choice which group key you wish to have VAUX attached too, my example pictures add the value to Group1 Key (see front panel of the meter for the Group1/2 keys). Select the desired tab.
  4. Click the insert button.
  5. Setup the value as this example:


    The VAUX value should show up in the list as below:




Last Revised:
Applies To:
Original Author: (recommended to place initials only)
Public
All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL191670 V1.0, Originally authored by KBAdPM on 04/12/2008, Last Edited by KBAdPM on 04/12/2008
Related ranges: ION Setup 2.1, ION Setup 2.0, 3720 ACM