המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
R034_How to adjust a motor current value less important than 0,4A on TeSysT

Goals and Symptoms

You can use TesysT for motor application which the current is less important than 0,4 amps. This document will describe you which parameters you have to modify to reach this area of current level.

Causes and Fixes

You can use TesysT for motor application which the current is less important than 0,4 amps. This document will describe you which parameters you have to modify to reach this area of current level.

Attachments

(Removed File URL: 198279_B6A2/R034_How_to_adjust_a_motor_current_value_less_important_than_0,4A_on_TeSysT.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/e588e16ba266cd29c125759800529e8d/fl_block_5/0.5DC?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL198279 V1.0, Originally authored by MiFo on 04/14/2009, Last Edited by MiFo on 04/14/2009
Related ranges: TeSys T

שניידר אלקטריק ישראל

קבצים מצורפים
R034_How_to_adjust_a_motor_current_value_less_important_than_0,4A_on_TeSysT.pdf [562.26 KB]