המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
On custom ION Enterprise Webreach screens some numeric objects are blank for the 3710 ACM and 3720 ACM meters.

This happens because some of the output values for this meter have the special character '#' in the label names. On the 37xx meters this cannot be changed. In order to get around the issue, link these outputs up to an arithmetic module in the VIP. Change the outputs of the arithmetic module to something without special characters (only letters and numbers) and then link the Vista diagram up to the newly created VIP arithmetic module outputs.

Date Created: October 24, 2008
Last Revised: May 6, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL198454 V1.0, Originally authored by MiNe on 05/07/2009, Last Edited by MiNe on 05/07/2009
Related ranges: 3720 ACM, 3710 ACM, ION Enterprise V5.6